Enterprise System Manager Shell

To open Enterprise Manager Shell in Windows, run Command Prompt as an administrator and change directories to the installation directory by running the following command: cd C:\Program Files\exacqvision\enterprisemanager \enterprisesystemmanager\ Then type: enterprisesystemmanager.exe shell To open Enterprise Manager Shell in Linux, open a Terminal window and type: sudo /usr/local/exacq/esm/enterprisesystemmanager shell <br> The following commands can be used… Continue reading Enterprise System Manager Shell

exacqVision Enterprise Manager Error When Saving Custom User Role

When attempting to make changes to an existing user role a warning banner pops up “Error while saving user role. Please try again.” To resolve copy the script “fix_userroles.py” to the EnterpriseSystemManager install folder. WindowsC:\Program Files\exacqVision\EnterpriseManager\EnterpriseSystemManager Linux/usr/local/exacq/esm/ Navigate to EnterpriseManager directory and Launch the Interactive shell Windows cd “C:\Program Files\exacqVision\EnterpriseManager\EnterpriseSystemManager” Linux Run the Script You… Continue reading exacqVision Enterprise Manager Error When Saving Custom User Role