Exacq Enterprise manager services on windows are not starting

Issue If Exacq Enterprise Manager services on Windows are not starting and giving this message Usually, it’s going to be a user privileges issue, and the user that is used for running the service is not able to start it Solution Sometimes in the domain environment, the service users will be restricted and will not… Continue reading Exacq Enterprise manager services on windows are not starting

Web Service – Services do not show up on install

When installing the web service the Service’s do not show up. The install seems if it completed successfully but does not create a service. After installing the latest version of the Webservice the control panel and service page looks like this: You can see the application installed but the services do not. Check to see… Continue reading Web Service – Services do not show up on install

Enabling DHCP services on exacqVision recorders

Description Starting in exacqVision 7.4, the option to enable Dynamic Host Configuration Protocol (DHCP) services is provided. A DHCP server is used to provide IP addresses to any device on the network that requests address assignment.In exacqVision this feature can be used to more easily assign proper IP addresses to cameras. If multiple DHCP servers… Continue reading Enabling DHCP services on exacqVision recorders