In various versions of exacqVision, version 8.8 and earlier, we have seen issues updating the IP settings on Linux servers using the exacqVision client. If you run into this issue, you can confirm the settings applied or change the settings using the method below. The exacqVision Client reads from the Interfaces file so if this… Continue reading Issues Updating IP Settings using the exacqVision Client
Tag: Servers
Using Remote Desktop to Manage Windows-based ExacqVision Servers
Remote Desktop allows you to connect to your Windows-based ExacqVision server over a network connection and operate it as if you were using the system directly. This can be especially useful when you want to upgrade the server software. Using Remote Desktop across public networks or the internet introduces many of the same security concerns… Continue reading Using Remote Desktop to Manage Windows-based ExacqVision Servers