Some systems may reboot immediately upon update or starting the server service when using 9.2.2. If the system experiences this it is likely to be due to the sysmgmtpi.dll (Windows) or sysmgmtpi.so (Linux). To resolve this you may opt to downgrade the server to 9.2.1 (currently available for download on website) or remove the sysmgmtpi… Continue reading Update to Server 9.2.2 Causes Continuous Reboot