Symptom In the exacqVision Client software on the ‘System Configuration’ page, under the ‘Date/Time’ tab, the Time Zone drop down menu has only one option, UTC-0. <br> Problem The user cannot set the proper server time zone. Affecting only Windows systems, the script that obtains the time zones from the operating system has failed. The… Continue reading Time Zone Only Shows UTC-0 Option
Tag: Server Time Zone
ESM Event Timestamp Incorrect After Time Zone Change
If you change the time zone on a system running Enterprise System Manager (ESM), the timestamp of ESM events might not match the time that the events actually occurred. <br> When ESM services are started, ESM reads the timezone configured in the operating system. If the system’s time zone is then changed, you must restart… Continue reading ESM Event Timestamp Incorrect After Time Zone Change