Server May Lose Network Connectivity When Bond Is Deleted

Symptom: exacqVision Server has lost network connectivity. <br> Problem: The settings from the deleted bond are arbitrarily applied to whichever interface was first alphabetically in the bond. All other interfaces in the removed bond are set to 0.0.0.0. If the alphabetically first interface is no longer physically connected, loss of network connection occurs. <br> Solution:… Continue reading Server May Lose Network Connectivity When Bond Is Deleted