ESM does not uniquely display multiple groups with the same name in rules engine

ESM does not uniquely display multiple groups with the same name in rules engine Effected platforms ESM 2.6 or greater <br> Symptom When multiple groups with the same name exist, the user may not be able to discern the individual groups when creating rules. On ESM versions before 3.6, all the servers that are on… Continue reading ESM does not uniquely display multiple groups with the same name in rules engine

ESM fails to process events due to server disconnect stop alert rule crashing the importer

Affected platforms exacqVision ESM 3.7.6 or later <br> Symptom If a rule is created to display an alert when the server disconnected state stops (that is, the server reconnects), the ESM importer will crash when that alert rule fires. To confirm, check the following logs: Open the log file logfile-importer and look for an entry… Continue reading ESM fails to process events due to server disconnect stop alert rule crashing the importer