Description Adding certain cameras with the wrong plugin type causes the exacqVision Server to go into a crash loop. Product Steps to Reproduce Expected Results Actual Results Solution NOTE: This has been specifically observed when Illustra cameras are added with Illustraflex instead of Illustra3 and Samsung cameras are added with Onvif instead of Samsung <br>
Tag: Server Crashes
exacqVision Server crashes and/or triggers watchdog reboot on system with no page file
Affected platforms Windows <br> Symptom If a page file does not exist on a Windows-based exacqVision system, one or more of the following symptoms may be encountered: exacqVision Server watchdog log message found in the server log. For example, 7/5/2015 12:02:54 AM tDVRpi Warning tDVR 0 proc 1 err -21 watchdog expired at 2015-07-05 04:00:28… Continue reading exacqVision Server crashes and/or triggers watchdog reboot on system with no page file