Must use unique UDP port for each DSC Neo panel a server connects to

Affected platforms exacqVision 7.4 <br> Description When integrating to a Neo panel using UDP configuration, in the exacqVision Client a UDP port number must be specified. Using the panel’s default will work for the first panel configured for that server. For all subsequent panels, first change the application UDP port number in the panel to… Continue reading Must use unique UDP port for each DSC Neo panel a server connects to

Getting server lists for exacqVision Client may connect to a server more than once

Description If there are two different servers with the same server name in two different groups in ESM, it is possible that the client sync with ESM will pull in the server at different times during the continuous sync with ESM (every 5 minutes) by confusing the group hierarchy of the same named servers.To workaround… Continue reading Getting server lists for exacqVision Client may connect to a server more than once