When adding an IP Serial Port, most of the time you will see the Status go to “Connected” However, the Type “TCP Listener” does not actually connect to the device sending data. We are simply opening up on that port and waiting for any unencrypted data to show up. Because of this the Status will… Continue reading TCP Listener not showing “Connected”
Tag: Serial Port
USBDIO and Serial Port Recovery
The following recovery enhancements have been added to exacqVision Server: USBDIO recovery enhancement: version 6.7.20.74529UART serial ports recovery: version 6.7.25.75004 <br> When a USBDIO or UART serial port device disconnects, exacqVision Server attempts to reconnect to the device after one second. If that attempt fails, the next attempt occurs after two seconds, and then four… Continue reading USBDIO and Serial Port Recovery