How to Determine the Age of a System Using a Serial Number

Exacq hardware serial numbers include both the year and the week number the system was built. See How to Find the Serial Number of an exacqVision System for help in finding your system’s serial number. There are a few different serial number prefixes depending on where the system was built. They are: After this, the… Continue reading How to Determine the Age of a System Using a Serial Number

How to Find the Serial Number of an exacqVision System

Using the Client Within the exacqVision Desktop Client application, click the Configuration (gear) icon from the top-left toolbar. Click on the ‘Systems’ node from the top of the left-hand side navigation tree. The grid displayed lists all systems added to this client. Find the ‘Serial Number’ column here. NOTE: Systems that are software only installs… Continue reading How to Find the Serial Number of an exacqVision System