Tag: Serial
TCP Listener not showing “Connected”
When adding an IP Serial Port, most of the time you will see the Status go to “Connected” However, the Type “TCP Listener” does not actually connect to the device sending data. We are simply opening up on that port and waiting for any unencrypted data to show up. Because of this the Status will… Continue reading TCP Listener not showing “Connected”
Crestron Serial
RS-485-to-USB Adapter Compatibility with ExacqVision
Two RS-485-to-USB adapters have been tested for compatibility with exacqVision: B&B Electronics, model 485USB9F-4W and VSCom, model USB-COMi-TB. The tests used the drivers supplied with the devices, and data has successfully been transmitted and received to and from each adapter. They were also tested in a loopback configuration with the RS-485 port built into an… Continue reading RS-485-to-USB Adapter Compatibility with ExacqVision
Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control
ExacqVision Hybrid servers have the ability to integrate with Pelco Coaxitron CXTA 9760 devices. This allows customers with existing Pelco PTZ cameras that are controlled through the coax with the Coaxitron protocol to be controlled using ExacqVision software. The CXTA accepts the Pelco 422 protocol from the ExacqVision server, and it outputs the data over… Continue reading Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control