Affected platforms exacqVision 4.12.3 to 7.0 <br> Symptom There is a small memory leak whenever the server executes a program. This leak is unlikely to cause a problem on any desktop systems, but it could cause a hang or reboot on Edge systems with limited memory, if the Edge server is configured to send frequent… Continue reading Internal memory leak when sending email