(NOTE: This article applies to hybrid ExacqVision systems with Stretch boards, manufactured from June 2012 to September 2013 as described in TAB 2013-01. If you need to replace the SATA power cable to an optical drive and hard drive please visit Article 2320.) <br> To replace a SATA power cable to a Stretch (sDVR) board in an… Continue reading Replacing SATA Power Cable in Hybrid ExacqVision Systems with Stretch (sDVR) Boards
Tag: SDVR Board
Re-installing an exacqVision Capture Card Driver
Important Beginning 12/14/2021 extension of the SSA “Software Subscription Agreement” will be restricted on systems which have an eDVR capture board. In addition, starting with exacqVision Server version 22.06 the XDVPI plugin has been removed and systems where the plugin is present will be blocked from upgrading. In order to either extend the SSA or… Continue reading Re-installing an exacqVision Capture Card Driver
exacqVision SDVR boards with PAL cameras
Sometimes exacqVision SDVR boards do not immediately recognize the PAL format of analog cameras. Images could be displayed in black and white or even with tearing. If your PAL cameras show those issues when using SDVR boards, complete the following steps in Linux: Log out of the restricted user account and log in as an… Continue reading exacqVision SDVR boards with PAL cameras