When connecting an NVR running Ubuntu 12.04 or older to a newer S-series you may have issues with it connecting and displaying the “Disconnected” message on the archiving page; even thou everything is correct and systems running Ubuntu 14.04 or newer DO NOT have this issue. When you search the logs, you will see a… Continue reading Archiving continually says “Disconnected” on Linux systems 12.04 and Older
Tag: Samba Shares
Configuring Samba (SMB) Shares on exacqVision S-Series Enterprise Could Fail After Repartitioning a Drive
If an exacqVision S-Series Enterprise system is configured for Samba (SMB) shares, and then the number of partitions on the drive is changed, configuring a Samba share on the new partitions could fail. <br> As a workaround, first configure the new partitions for extended storage to ensure that partitions are properly formatted. <br>