SMB server signing and encryption for Archiving

exacqVision’s default method for archiving recorded data uses the SMB protocol. Using an exacqVision S-Series storage system makes configuring archiving simple. Users may also archive to SMB shares configured on their own third-party systems, but installing and configuring Samba or SMB Shares on non-Exacq built systems is outside the scope of Exacq Support. There have… Continue reading SMB server signing and encryption for Archiving

Auto Export to a Network Share from Linux-based Exacq Server

To configure auto export from a Linux-based Exacq Server to a network share, complete the following steps: (Windows procedure here)<br><br> NOTE: For Linux-based systems, this procedure is available in exacqVision Server/Client version 6.6 and later.<br><br> To remove the network target, complete the following steps: <br>

Auto Export to Windows Network Share from Windows-based Exacq Server

On a Windows system, exacqVision Server runs as a service. This is desirable because the service starts recording video without user interaction when the system is started. However, this creates an issue with the management of credentials for access to network storage, as the exacqVision Server does not run from a normal user account that… Continue reading Auto Export to Windows Network Share from Windows-based Exacq Server