If the camera is connected to ExacqVision Server and showing connected on the add IP camera page but not streaming videos and showing acquiring video. That means the RTSP streaming port may need to be opened on the Firewall, normally 554
Tag: RTSP Stream
How do I open an RTSP stream in VLC?
VLC is a good tool to use if you are having issues with an IP camera. If the camera can provide you with RTSP stream data, you can display that stream in VLC and see if you have the same issues you experience with the camera ExacqVision. This helps troubleshoot an issue because it removes… Continue reading How do I open an RTSP stream in VLC?