Learn to use the embedded RTSP Server to provide video streams to external services.
Tag: rtsp server
RtspserverPI may fail to re-stream JPEG video
Issue When re-streamed to third-party RTSP client applications, JPEG video may fail to be decoded, due to our incorrect JPEG header processing. Version affected 19.12 Workaround Re-stream as any other codec. Fixed Version 20.12 or later
SCN-00000004 – exacqVision RTSP Server
SCN #SCN-00000004Title of SCNexacqVision RTSP ServerTRAC #Effective Version2018-03 Integration / 19.12 PluginProducts AffectedIntegrationReason for Change (Summary)2021-03 – updated to reflect built-in plugin features Change The “exacqVision RTSP Server” was available as a side integration beginning in March of 2018. As of the 19.12 release, these functions have moved into a built-in plugin called ‘rtspserverpi’. The… Continue reading SCN-00000004 – exacqVision RTSP Server