Categories
Knowledge Support Support exacqVision Server Categories Products

Second Reviewer

Second Reviewer is a feature available for highly sensitive areas which requires two users to authenticate in order to access recorded video.

This feature is hidden by default, and requires a special configuration file to make it visible.

  1. This configuration file is available at this link for download: activatesecondreviewer.settings<br><br>
  2. The configuration file is imported using the Import button at Configure System > System tab > Settings > Import

    NOTE: Once imported the Second Reviewer feature cannot be undone. You should consider backing up your server configuration prior to performing this import.<br><br>
  3. After importing the settings file, navigate to the Security tab. This will display new fields.

    <br><br>
  4. Check the Enable box and complete the fields for first and second reviewer passwords, then select the functions this is required for.
    • Live
    • Search
    • Export<br><br>
  5. Click Apply. A warning will appear advising you that these passwords will be required to access the checked items or to make changes in the future.
    <br><br>
  6. The exacqVision Desktop Client will prompt for both password when performing tasks that require using the functions you selected.<br><br>


NOTE: When Second Reviewer is enabled:

  • Archiving, auto export profiles, and email notification attachments such as .jpg and .mov files are disabled.<br><br>
  • Video preview may not be available on configuration pages.<br><br>
  • Using the exacqVision Web Client and Exacq Mobile 3 with any Second Reviewer function enabled is not supported as there is no way to authenticate via the web interface.

<br>