Problem If multistreaming is enabled on an Illustra Flex camera, you cannot use ExacqVision Client to change the resolution on any stream except for the last stream added. Affects firmware earlier then 3.0.5. Workaround If you want to change the resolution on a previously added stream, you must first delete any streams added after that… Continue reading Changing the Resolution of additional streams Illustra Flex Cameras
Tag: Resolution
Enabling 4×3 Resolution to Eliminate Gray Bars in Video Windows (Legacy)
NOTE: These are Legacy instructions. This behavior was replaced when Client settings implemented Panel Size settings.When using cameras with a 4×3 resolution, gray bars might appear to the left and right of the camera’s video window in exacqVision Client. To stretch the 4×3 video so that it fills the screen, manually set the video card… Continue reading Enabling 4×3 Resolution to Eliminate Gray Bars in Video Windows (Legacy)
Get the Monitor Size (resolution) Back for Linux Sy stems
The monitor can get stuck in 640*480 mode if the system is booted with no monitor connected. To get the monitor size back for Linux systems, complete the following steps after opening Terminal: Type cd /etc/X11Type sudo mv xorg.conf xorg.bak.confRestart the system with a monitor attached. <br>