*** INTERNAL USE *** If you are unable to login to the ExacqVision software and need to reset the password, perform the following: WARNING: This will remove ALL user accounts from the configuration, not just the admin locked out. Windows OS 1. Visit the following page and download the server version you need.https://www.exacq.com/reseller/legacy/?file=Legacy/index.html2. On a… Continue reading Exacq Client Username/Password Reset
Tag: Reset
exacqVision – Resetting the Operating System Password
Title exacqVision – Resetting the Operating System Password Description How to reset the OS password on an ExacqVision Server Product exacqVision Server Solution Either a full re-image or an on-board system recovery will need to be performed to reset the operating system password. Knowledge Base Article #935 “System Recovery using on-board recovery partition”
Enterprise System Manager Shell
To open Enterprise Manager Shell in Windows, run Command Prompt as an administrator and change directories to the installation directory by running the following command: cd C:\Program Files\exacqvision\enterprisemanager \enterprisesystemmanager\ Then type: enterprisesystemmanager.exe shell To open Enterprise Manager Shell in Linux, open a Terminal window and type: sudo /usr/local/exacq/esm/enterprisesystemmanager shell <br> The following commands can be used… Continue reading Enterprise System Manager Shell
How to reset the ESM admin password
Description If the ESM administrator has lost or forgotten the ESM admin password, it can be reset by executing shell commands in the operating system of the ESM machine. Note: root/admin level access to the ESM machine is required for this process. In Linux: Open bash shell as root, or provide sudo on command executionNavigate to… Continue reading How to reset the ESM admin password