If you have an Linux-based exacqVision system (such as exacqVision EL) that requires SDVR drivers, but you mistakenly installed XDVR drivers, you must remove the XDVR drivers before installing the SDVR drivers. There are two equal ways to remove the XDVR drivers; use the one that you prefer or have better access to: In Terminal,… Continue reading Replacing XDVR drivers with SDVR drivers on Linux-based exacqVision Systems
Tag: Replacing
Adding or Replacing Hard Drives with exacqVision EL Servers Running Ubuntu 10.04 or earlier (Legacy)
Steps: <br>