Replacing a Drive in Ubuntu 20.04 or later, Using GParted (Legacy)

This procedure is applicable to replacing the primary hard drive of a Linux-based exacqVision system. It assumes that the operating device is installed to an on-board flash device. Do NOT use this procedure when simply adding a drive to a system.

ExacqVision A-Series 4U Drive Replacement Guide

NOTE: This article assumes that you already know which drive number must be replaced, and that you have a replacement drive ready to install in the system.NOTE: The photos in this article illustrate the replacement of Drive 3.To replace a hard drive in an exacqVision A-Series 4U system manufactured on or after 07/30/2015, complete the following steps:… Continue reading ExacqVision A-Series 4U Drive Replacement Guide