Title Windows Remote Desktop Connection/RDP Not Working Description This has been observed after the Operating system has been updated to Windows 10 on exacqVision Servers using the Win10 upgrade kit. Product Windows 10 Remote Desktop Connection RDP Solution Make sure you have run the Deploy clean-up script as per the exacqVision field recovery instructions. Check the desktop and… Continue reading Windows Remote Desktop Connection/RDP Not Working
Tag: Remote Desktop
Using Remote Desktop to Manage Windows-based ExacqVision Servers
Remote Desktop allows you to connect to your Windows-based ExacqVision server over a network connection and operate it as if you were using the system directly. This can be especially useful when you want to upgrade the server software. Using Remote Desktop across public networks or the internet introduces many of the same security concerns… Continue reading Using Remote Desktop to Manage Windows-based ExacqVision Servers