2024-09 September Quarterly Release Training

<br> exacqVision Server exacqVision Client exacqVision Web Service exacqVision Enterprise Manager Exacq Mobile 3 exacqVision Mobile Exacq Hardware Hardware Revisions exacqVision Advantage Illustra <br>

2024-03 March Exacq Release Training

This training covers the following topics: Quick Add – Requires exacqVision Server and Client 24.03 or higher. Supports only Illustra Flex and Pro Gen 3/4 cameras. Architecture changes – Changes made in how the new exacqVision Mobile app connects to exacqVision Server and when exacqVision Web Service is still required. Remote Connectivity – Provided for… Continue reading 2024-03 March Exacq Release Training

2023-09 September Quarterly Release Training

<br><br> ExacqVision Server Bug Fix – Fixed issue causing server crash due to missing microSD card in Illustra multisensor cameras.If camera has no microSD for one sensor, but does for another, network loss recording action caused a crash. (AESW-7549) Bug Fix – Prevent offload from Illustra BWC from hanging Bug Fix – If camera does… Continue reading 2023-09 September Quarterly Release Training

2023-06 June Quarterly Release Training

ExacqVision Server Bug Fix – Fixed excessive Archiving status messages (AESW-4989) Bug Fix – Debian installer no longer enabled eventpi by default Bug Fix – Fixed issue capturing all metadata when multiple events are sent as one alarm Bug Fix – Ensure eventpi database is purged after server reboot Bug Fix – Fixed connection status… Continue reading 2023-06 June Quarterly Release Training

2023-03 March Quarterly Release Training

ExacqVision Server Bug Fix – Fixed PTZ preset administration for custom users to create presets for analog cameras (AESW-4357) Bug Fix – Fixed monitoring RAID background tasks, like consistency checks and background initialization (AESW-4387) Bug Fix – Fixed reporting incorrect RAM, was displaying MB instead of GB (AESW-2498) Bug Fix – actipi – Reduce metadata… Continue reading 2023-03 March Quarterly Release Training

2022-12 September Quarterly Release Training

ExacqVision Server Bug Fix – Fixed issue preventing archiving of analog video to Cloud Drive Bug Fix – Motion Detection not working on Holis cameras Bug Fix – Corrected issue setting NTP server for illustra3pi and illustramultipi camera plugins Bug Fix – Fixed issue with missing frames from PTZ cameras causing image tearing in recorded… Continue reading 2022-12 September Quarterly Release Training

2022-09 September Quarterly Release Training

*There appears to have been a slight bug in the presentation recording where the video recording did not capture the videos being played on the screen. The links below will provide access to the PowerPoint file and individual demonstration videos. ExacqVision Server Bug Fix – Removed limit of 256 devices displayed for Access Control plugins,… Continue reading 2022-09 September Quarterly Release Training

2022-06 June Quarterly Release Training

ExacqVision Server Bug Fix – Fixed issue preventing DMP device from being deleted Bug Fix – Fixed plugins that could potentially cause system stall during shutdown Bug Fix – Fixed problem wherein adding Illustra devices with Onvif caused flood of configuration messages to logs Bug Fix – Fixed problem with SSO if AES encryption enabled… Continue reading 2022-06 June Quarterly Release Training

2022-03 March Quarterly Release Training

exacqVision Client  * Enhancement – Show toast for all web panels that fail cert setting checks.  * Enhancement – Added separate archive rate and upload rate fields for archive targets that report them.  * Enhancement – Add Enter to the default DCZ joystick profile  * Enhancement – Added Select Camera joystick button action  * Enhancement… Continue reading 2022-03 March Quarterly Release Training

2021-09 September Quarterly Release Training

Feature: Client – Enhancement – Restricted view windows. – #21926Server – Feature – Restricted view windows. – #22863Exports only allowed for .psx and .exeRequires password to hide – on a timer (5 minutes) Client Enhancement – macOS – Force client into dark theme to match OS setting.Enhancement – Ability to password protect and encrypt exe… Continue reading 2021-09 September Quarterly Release Training