Operating System Release Notes

Systems built by Exacq utilize customized OS images for Windows and Ubuntu (Linux). There may be instances where it is necessary to check the release version on an Exacq system. The release notes are contained within the operating system in a text file titled Release_Notes located on the root of the OS drive. File path… Continue reading Operating System Release Notes

Cloudvue 22.9.1 Technical Release Notes

Description  Cloudvue Release 22.9.1 is a defect/fix release Product  Cloudvue Deployed InstanceDateNorth America03/08/2023Australia03/13/2023EMEA03/13/2023 Enhancements/Fixes “Force Certify” buttoned added the Cloudvue Manager (CVM) user Interface when the device is offline. Devices with certificate problems appear as offline. This fix provides the CVM a method to assign a certificate while the device is offline. People/Vehicle detection restored to… Continue reading Cloudvue 22.9.1 Technical Release Notes