Description Exacq cloud hosted relay service eliminates the need for most firewall configuration and prevents exposing the NVR directly to inbound internet traffic via port forwarding by creating a unique relay URL as a proxy to access the NVR. Product Prerequisites Solution Troubleshooting In the event the Relay URL is missing or having any other… Continue reading Enabling and Troubleshooting exacqVision Web Server Relay Service
Tag: Relay
ExacqVision Web Service Fails to get Public URL from Relay Manager
Summary The OpenSSL Certificate from Ubuntu that the relay service utilizes is expired Description Error failed to get public URL from relay manager rpc error: code = Unavailable desc = connection error: desc = “transport: authentication handshake failed: x509: certificate has expired or is not yet valid: current time 2022-02-24T10:19:29-08:00 is after 2021-09-30T14:01:15Z” wfe 32563… Continue reading ExacqVision Web Service Fails to get Public URL from Relay Manager
ExacqVision Web Server Relay Service Issue
Description How to diagnose if the Fast Reverse Proxy Client (FRPC) is the source of issues with the ExacqVision Web Server relay service. Product ExacqVision Web Server Troubleshooting FRPC FRPC provides a proxy service for Relay Connections used by ExacqVision Web Server. This eliminates the need for firewall configuration and prevents exposing the NVR directly… Continue reading ExacqVision Web Server Relay Service Issue
Automation Control Circuitry
What is TTL? TTL stands for Transistor-to-Transistor Logic, where the “logic” determines which values are high and low. Standardized common TTL circuits operate with a 5-volt power supply. A TTL signal is defined as low when the voltage is measured between 0.0 V and 0.8 V with respect to the ground terminal, and high when… Continue reading Automation Control Circuitry