Recording Not Possible – Windows DST Issue

Description  If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST).  Use the following instructions to verify and resolve the issue.  Product  Solution These instruction are based on Windows… Continue reading Recording Not Possible – Windows DST Issue

‘Recording Not Possible’ Status on ExacqVision Edge Illustra

Description The status of the storage page is showing “Recording Not Possible” on ExacqVision Edge for some Illustra cameras.  This is a result of SD encryption mode being enabled on the camera.    Products Steps to Reproduce  Install the Edge software on the camera, and then try to record video to the SD card.  Expected… Continue reading ‘Recording Not Possible’ Status on ExacqVision Edge Illustra

Recording Not Possible – Linux DST Issue

Title Recording Not Possible – Linux DST Issue Description  If the exacqVision Server data drives are full and are displaying “Recording Not Possible” on the storage page then it is possible an invalid hour folder was created during the switch to Daylight Savings Times (DST).  Use the following instructions to verify and resolve the issue. … Continue reading Recording Not Possible – Linux DST Issue

Server not recording to iSCSI volumes

Description:If all the storage drives are ISCSI, then “Recording Not Possible” is seen on the Storage page of the desktop client.If some storage drives are local, then recording only happens to local drives, thus reduces the overall content age of the oldest available video/audio.Workaround: Fixed Version:21.03.107 Back patched and available in 21.03.7