Title exacqVision sysprep Error “Failed to Write Model number” Description During a full re-image of an exacqVision Server, while doing the sysprep, an error occurred “failed to write the model number” (see Figure 1) Product exacqVision Server Solution It was discovered that the integrator was using the wrong iso file for the… Continue reading exacqVision sysprep Error “Failed to Write Model number”
Tag: Re-Image
Windows Remote Desktop Connection/RDP Not Working
Title Windows Remote Desktop Connection/RDP Not Working Description This has been observed after the Operating system has been updated to Windows 10 on exacqVision Servers using the Win10 upgrade kit. Product Windows 10 Remote Desktop Connection RDP Solution Make sure you have run the Deploy clean-up script as per the exacqVision field recovery instructions. Check the desktop and… Continue reading Windows Remote Desktop Connection/RDP Not Working
Retail Key Image Release Highlights – 202108
August 27,2021 New and updated zip files are now available on the public website https://www.exacq.com/support/downloads/Username: guest Password: exacqvisionip Highlights: Introduced Ubuntu 20.04 (18.04 is now deprecatedUpdated field recovery instructions are packaged within the zip filesThe following motherboards do NOT support Ubuntu 20.04 and servers with these motherboards that need to be re-imaged must use Ubuntu 18.04/RETAIL1804-21.03.5.zipQ87MAH81-X1D180SD190SD290S… Continue reading Retail Key Image Release Highlights – 202108