Description exacqVision displays a value 1-100 for motion sensitivity. The camera itself only uses a 1-10 scale. When the user sets the sensitivity to 23, the actual value maps to 2, but the GUI still displays 23. If the camera is deleted and re-added, the sensitivity would display 20, rather than 23. <br>