Description:- Some of the drives on the raid system are not working on the same raid array with the other drives even if it’s Identical, except the logical sectors showing 512b for the majority and 4K for the new drive or vice versa, so to convert this drive, you will need to use a unique… Continue reading How to change the logical sectors of WD HDDs
Tag: RAID Drives
Storage
This video will introduce you to the controls available on the Storage page, which allow you to monitor the health and control which drives are written to. Gain an informed understanding of the Expiration Configuration settings and the retained amount of data stored on your system. Use the Extended tab to optionally connect to a… Continue reading Storage
RAID drives show threshold exceeded on Linux
Description On server version 8.9.25 or newer, RAID drives may show threshold exceeded error on Linux systems. Some windows systems may also show this depending on the raid controller and drive model. <br> Workaround Add following rows to hwmconfig.xml file under <SmartConfig> section Fix will be available in v9.1.1