Title Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Windows Description MSM has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228). As a result you may be able to replace MSM with LSA using the following instructions. Product … Continue reading Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Windows
Tag: RAID Controller
Dirty Cache not allowing OS to boot
If a customer calls with a system not booting and is prompted to hit X to clear the Cache, please see this forum on current suggestions and provide feedback. https://forum.exacq.com/t/current-issue-dirty-cache/74 Note: This has not been fully root caused yet but recommendations can be found here:
Replacing a Drive on an exacqVision System with an LSI RAID Controller
It is considered best practice to periodically check the health and status of exacqVision storage devices. If a device has failed, this guide explains the steps needed to replace that device using exacqVision Client and LSI MegaRAID Storage Manager. <br> Identify and Replace the Failed Drive <br> Add the New Drive to the Array <br>… Continue reading Replacing a Drive on an exacqVision System with an LSI RAID Controller
Highpoint RAID Troubleshooting (Legacy)
For troubleshooting information, see the attached PDF.The following exacqVision models were manufactured with Highpoint RAID controllers from 2007 to 2009: <br> To determine whether your system contains a Highpoint RAID controller, look at the RAID BIOS screen that appears when the system is first started (before the operating system starts). <br>