Push notifications provide the ability to alert users of events even when they do not have the Exacq Mobile 3 app open. There are two options for Push Notifications, those triggered by camera analytics and analytic appliances, and those triggered by other types of events, which require the use of Event Monitoring. Both options are… Continue reading Enabling Exacq Mobile 3 Push Notifications
Tag: Push Notifications
Recording must be configured to retrieve video thumbnail for analytic push notifications
Description Exacq Mobile 3, version 19.09, allows a user to subscribe to and receive push notifications for triggered analytic rules. As part of this feature, showing the details for an analytic notification in the app will show a frame from the associated camera (if there is one) at the time of the event. In order… Continue reading Recording must be configured to retrieve video thumbnail for analytic push notifications
Exacq Mobile 3 missing push notifications settings
In the Exacq Mobile 3 application a user can configure Push Notifications in the Push notifications sections of the settings page.The following are the scenarios where the Push Notifications settings will not be shown and the user will not be able to use the Push Notifications feature of the Exacq Mobile 3 application: <br>