Allibi Camera ALI-PZ40-UZAI PTZ is disabled by default on 23.06-24.03

Description  Cameras are not able to switch to Serial IP under Mechanical tab.Looking at the Onvif plugin the PTZ for the camera was set to “0”We could not enable it in the client. When attempting to set the serial to IP in the mechanical PTZ tab, it would flip back to the Serial Port to… Continue reading Allibi Camera ALI-PZ40-UZAI PTZ is disabled by default on 23.06-24.03

Camera Settings

Nested in the configuration tree, beneath Camera Recording, is the list of all cameras connected to the system. Clicking on any of these cameras will display the settings page for that individual camera. From here, you have access to important settings, such as the camera name, configuring the optional on-screen display (OSD), picture settings, motion… Continue reading Camera Settings

Samsung PTZ functionality loss in exacqVision Server 20.03

Issue  Samsung PTZ functionality loss in exacqVision Server 20.03 <br> Workaround Re-enable mechanical PTZ for the camera, via exacqVision Client. <br> Version Affected 20.03 <br> Version Fixed Fixed in 20.03.111 and forthcoming 20.03.7 RC