Substitute Power Supply Exceeding Voltage Range on 2U Z-Series

Description  Manufacturing has had to substitute a power supply which has been observed to exceed the originally specified operating range.  Product  exacqVision 2U Z-Series Servers Solution To resolve update to exacqVision Server version 22.06.104 or higher available in Artifactory. The allowable voltage range has been changed from 11.4 – 12.6 VDC to 11.1 – 12.9… Continue reading Substitute Power Supply Exceeding Voltage Range on 2U Z-Series

Resetting the Power Supply Alarm

Description  Exacq built systems with redundant power supplies will emit an audible alarm in the event of a power failure. Here is how to silence the various models so you can enjoy peace and quiet while determining the cause of the failure. Product  Solution The following photos show the location of the mute button on… Continue reading Resetting the Power Supply Alarm