PSMOVE For Windows

Description  The purpose of this KB is to help run PS MOVE and where to place the files on a system. Product  PSMOVE.exe Exacq Server 23.03 and above. File Location:  Windows:Place psmove.exe in the Server folder.Open powershell or command promt as ADMIN.cd C:\Program Files\exacqVision\Server and place the psmove.exe into the server folder. Linux: ETA not… Continue reading PSMOVE For Windows

Psmove may get frozen on windows machine

*** INTERNAL USE *** Description  When using psmove on a windows machine the process may get frozen and you will get a cursor in PowerShell that stops blinking. This issue will occur if psmove is trying to move data to a date that does not exist in the local storage. Product  Any ExacqVision NVR running… Continue reading Psmove may get frozen on windows machine

Running psmove on Ubuntu Linux

*** INTERNAL USE *** Description  The psmove utility was designed to move psfiles to the correct location after a time zone change or if a files time does not match frame times.  It will perform a search on all local storage drives, read the PSI file header for the start time, determine if the PSI… Continue reading Running psmove on Ubuntu Linux