Green Lock and Gear Icons in the exacqVision Client

Description  A green icon indicates a secure (HTTPS) connection is being used for either or both the configuration connection to the device and/or the video stream.  Product  exacqVision Client Solution The green lock and gear icons are used as a visual indicators of the connection protocol being used by the camera.  They can be found… Continue reading Green Lock and Gear Icons in the exacqVision Client

SMB server signing and encryption for Archiving

exacqVision’s default method for archiving recorded data uses the SMB protocol. Using an exacqVision S-Series storage system makes configuring archiving simple. Users may also archive to SMB shares configured on their own third-party systems, but installing and configuring Samba or SMB Shares on non-Exacq built systems is outside the scope of Exacq Support. There have… Continue reading SMB server signing and encryption for Archiving

What analog PTZ protocols does Exacq support?

Exacq supports the following RS-422 and RS-485 PTZ protocols. With each protocol, you can specify the baud rate, data bits, stop bits, parity, flow control, and maximum line length. ProtocolSupported PTZ PresetsAD-M320096AD-M3200 Multi96AD-MP4896AD-MP48 Multi96AD-RS42296Bosch (OSRD)99GE-ASCII64GE-Impac32HSD-Pelco-D128Panasonic64Pelco-D32Pelco-P32 <br> NOTE: Devices that require the use of other protocols, not listed above, may still be used with supported encoders.… Continue reading What analog PTZ protocols does Exacq support?