Mobile OEM Toolkit produces invalid iOS packages when the OEM does not include support for Push Notifications

Affected platforms Mobile OEM Toolkit v1.3.1.8525 <br> Symptom If an OEM is attempting to create an iOS package using the Mobile OEM Toolkit v1.3.1.85257 and does not have their iOS provisioning profile set up for Push Notifications, the OEM will be unable to submit the application to iTunes Connect.This script error will cause the web… Continue reading Mobile OEM Toolkit produces invalid iOS packages when the OEM does not include support for Push Notifications