Description Manufacturing has had to substitute a power supply which has been observed to exceed the originally specified operating range. Product exacqVision 2U Z-Series Servers Solution To resolve update to exacqVision Server version 22.06.104 or higher available in Artifactory. The allowable voltage range has been changed from 11.4 – 12.6 VDC to 11.1 – 12.9… Continue reading Substitute Power Supply Exceeding Voltage Range on 2U Z-Series
Tag: Power Supply Alarm
Power Supply Alarm False Trigger
Problem After an upgrade the server emits a Power Supply Alarm which is false. This happens on units with DIO boards. When the server is connected to EM a power supply alarm is triggered every 15 minutes. Solution This issue occurs due to a variable stuck in the sysmgmtpi.xml file. To resolve this the sysmgmtpi… Continue reading Power Supply Alarm False Trigger
Resetting the Power Supply Alarm
Description Exacq built systems with redundant power supplies will emit an audible alarm in the event of a power failure. Here is how to silence the various models so you can enjoy peace and quiet while determining the cause of the failure. Product Solution The following photos show the location of the mute button on… Continue reading Resetting the Power Supply Alarm