EM Camera Permission in Postgres DB Causing High CPU usage for the Importers

Description  Some customers might have High CPU usage on their EM servers. In which the CPU runs at 100%. Product  EM- Version 23.0.3 and older. Steps to Identify the Cause  Log into the EM server and validate that the importers are running hard. Normally there will be several importer services opened and being used. You… Continue reading EM Camera Permission in Postgres DB Causing High CPU usage for the Importers

exacqVision Default Ports

Description  The following is a list of default port numbers used by exacqVision software. NOTE: Many ports listed below may only used with certain configurations or by optional services and integrations. Products Port List PortDescription25Simple Mail Transfer Protocol (SMTP)80exacqVision Web Server/exacqVision Enterprise Manager (HTTP)How to change Web Service portsHow to change EM web ports389LDAP (Lightweight… Continue reading exacqVision Default Ports

Setup Postgres with SSL

Description After Postgres is installed and an SSL certificate is acquired: 1. Open the postgresql.conf for editing as an administrator:Windows: C:\exacqVisionEsm\PostgreSQL\9.2\data\postgresql.confLinux: /usr/local/exacq/esm/PostgreSQL/9.2/data/postgresql.conf2. Locate the “# – Security and Authentication -” section:Replace it with:# – Security and Authentication – #authentication_timeout = 1min # 1s-600s ssl = on # (change requires restart) #ssl_ciphers = ‘DEFAULT:!LOW:!EXP:!MD5:@STRENGTH’ # allowed SSL ciphers # (change… Continue reading Setup Postgres with SSL