Using the Serial Ports page allows you to configure your ExacqVision system to receive serial data from Point of Sale (POS) devices, ATMs, access control devices, and more over UART or serial over IP connections. Learn more about the address, ports, and protocols used for these tasks.
Tag: POS
exacqVision SDK / API and OEM Solution Partner Requests
Title exacqVision SDK / API and OEM Partner Solutions Summary exacqVision SDK & OEM Solutions, we are part of the Connected Partner Program, so all request must first register via the Connected Partner Portal to be considered. Description Exacq Technologies provides integration tools that enable dealers and development partners to rapidly integrate external devices and… Continue reading exacqVision SDK / API and OEM Solution Partner Requests
Search for Serial Data unexpectedly fails to return results
Description When set to record, exacqVision Server stores serial data in a database called pospi.db Default locations are: After verifying that serial data is configured correctly and data is being received if searches fail to return results for serial events check the exacqVision Server logs for entries similar to the following. These messages are indicating… Continue reading Search for Serial Data unexpectedly fails to return results
exacqVision POS-ATM Information Guide
Requirements*This document applies to exacqVision 4.3 and later.*Serial data can be received using RS-232, HTTP, or TCP/IP. The data must be in an un-encrypted ASCII format. Formatting such as .xml can be used, but the data cannot be parsed.*If there are questions the data format, see sections 4 and 5. <br>exacqVision Serial Data Capabilities Serial data is… Continue reading exacqVision POS-ATM Information Guide