SCN #SCN-00000009Title of SCN‘Poll Error’ drive statusTRAC ##15439Effective Version9.4 – 9.6Products AffectedServerReason for Change (Summary)Eliminating false positive ‘Offline’ drive status in Linux Change Because of the way Linux handles how processes can trigger other sub-processes, certain features would fail if the ‘core’ process was utilizing more than 50% of its available memory. In exacqVision 9.2… Continue reading SCN-00000009 – ‘Poll Error’ drive status