Dealer Gateway Setup Quick Start
Tag: PoE
PoE Interfaces Created on Non-PoE Server
Symptom: After importing a configuration file, PoE interfaces appear on a machine with no PoE interfaces. <br> Problem: Configuration exports are primarily intended for backing up configuration of the same machine, not for migrating a configuration to another piece of hardware. When importing a configuration file from a PoE capable device (M-series or Una LC),… Continue reading PoE Interfaces Created on Non-PoE Server
exacqVision G-Series PoE Network Video Recorder
Connecting cameras over 100m in distance from G-Series PoE or Una recorders
ExacqVision G-Series PoE and Una recorders provide Power-over-Ethernet (PoE) ports for direct connections to cameras, rather than accessing cameras through a switched network. The TIA/EIA 568 standard provide that the maximum allowable length of a Cat5/5e or Cat6 cable is 100 meters (328 feet) for ethernet networks. To connect a camera farther than 100m away,… Continue reading Connecting cameras over 100m in distance from G-Series PoE or Una recorders