Video may be exported from exacqVision in different formats. The table below illustrates some of the differences in these formats. Multi-Camera: For the purposes of this article, multi-camera means many camera streams are combined into a single exported file. When exporting as .MOV, .AVI, or .MP4 each stream will end up as its own file.… Continue reading exacqVision Export Video File Types
Tag: Playback
Why can’t I play back video from my 5 Megapixel cameras after export?
Some media players, such as Windows Media Player, have problems when playing back full 5 Megapixel MJPEG video images in the AVI format. This is a limitation of the default codecs in the media players, and it applies to both exports from the server and already exported EXE files. <br> One solution is to download… Continue reading Why can’t I play back video from my 5 Megapixel cameras after export?