Description The Force TCP option forces the video stream to be sent using TCP/IP. This is recommended when live video is either displaying artifacts, video tearing, is heavily pixelated or a blue or green screen is being displayed. Product Solution
Tag: Pixelated Video
Issue in client with higher resolution cameras
When using a 4K camera with a resolution of 8192X1728 or 4096X864 the video is pixelated. Changing the resolution of the camera to 2048X432 or lower shows the image unpixellated. This will be fixed in the December quarterly Client release 21.12.X **Observed on Axis Q3819-PVE**
Pixelated Video on Bosch ONVIF Cameras
If live video from a Bosch ONVIF camera displays pixelization in exacqVision Client, complete the following steps: Browse to the camera’s advanced mode Encoder Profile page.Ensure that IP is selected in the GOP Structure drop-down list.Ensure that the I-frame Distance slider is configured for a low number (10, for example).Ensure that I-frame Quality and P-frame… Continue reading Pixelated Video on Bosch ONVIF Cameras