The following recovery enhancements have been added to exacqVision Server: USBDIO recovery enhancement: version 6.7.20.74529UART serial ports recovery: version 6.7.25.75004 <br> When a USBDIO or UART serial port device disconnects, exacqVision Server attempts to reconnect to the device after one second. If that attempt fails, the next attempt occurs after two seconds, and then four… Continue reading USBDIO and Serial Port Recovery
Tag: Peripherals
Removing an Unwanted USB I/O Device from a Server’s Configuration
If a USB I/O module was previously used and later disconnected from the server, the software will retain the configuration and the module will remain listed in the left-side navigation panel. If you wish to permanently remove this device from appearing in the software, you will need to log in to the server’s operating system… Continue reading Removing an Unwanted USB I/O Device from a Server’s Configuration
RS-485-to-USB Adapter Compatibility with ExacqVision
Two RS-485-to-USB adapters have been tested for compatibility with exacqVision: B&B Electronics, model 485USB9F-4W and VSCom, model USB-COMi-TB. The tests used the drivers supplied with the devices, and data has successfully been transmitted and received to and from each adapter. They were also tested in a loopback configuration with the RS-485 port built into an… Continue reading RS-485-to-USB Adapter Compatibility with ExacqVision
Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control
ExacqVision Hybrid servers have the ability to integrate with Pelco Coaxitron CXTA 9760 devices. This allows customers with existing Pelco PTZ cameras that are controlled through the coax with the Coaxitron protocol to be controlled using ExacqVision software. The CXTA accepts the Pelco 422 protocol from the ExacqVision server, and it outputs the data over… Continue reading Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control
Does the ExacqVision Client Support Multiple Monitors?
Yes, ExacqVision Client supports multiple monitors. We have tested up to four VGA monitors from a single workstation. Typically, a user will run one instance of the ExacqVision Client per monitor. Because decompressing video is CPU-intensive, we recommend one core per Client for the best user experience. To drive up to four VGA monitors, we… Continue reading Does the ExacqVision Client Support Multiple Monitors?
What types of microphones are compatible with the ExacqVision Hybrid NVR?
When using the audio input terminals on the rear of an ExacqVision Hybrid NVR, you will need a microphone with a a pre-amplifier capable of producing a line level output that can be connected directly to the ExacqVision audio terminal inputs. If using a mic level output microphone, you will need a mic pre-amp to… Continue reading What types of microphones are compatible with the ExacqVision Hybrid NVR?
Can I use a Joystick with exacqVision Client software instead of a mouse?
Yes. Exacq offers the exacqVision Surveillance Keyboard for this purpose. <br>