Description Pelco Optera is a multi-sensor 180/360 camera that provides panoramic views. We started supporting this model with r101894 dev build 7.9.32.101939 and officially in 8.0.0.102418 RC. <br> Fix The camera should be set to the “Panomersive Uni-stream” mode.In the camera web page, got to the “System” tab and under “Optera Compatibility Mode”. Let the camera reboot… Continue reading Pelco Optera supports Panomersive Uni-stream mode