A Pelco Pro Sarix camera (IMP-1110) failed to send motion notifications on a Windows Server 2012 system running the the Explicit Congestion Notification (ECN) service. The ECN service and Pelco plugin use the same TCP port 8575; if the ECN starts automatically after system startup, the notification subscription from the Pelco plugin can fail, meaning… Continue reading Pelco Motion Notification Could Fail on exacqVision System with Windows Server 2012