Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq

Description  The Pelco SMLE1-15V5-3h does will not record or see last motion events in exacq client/ server.Both Firmware’s were tested and work with the override.4.80.0.24(F722c136)and fw 4.86.0.20(7a7d6563) Product  ExacqVision Server 24.03.7.0 – 24.09.4.0 Steps to Reproduce  Set up motion in the cameras gui for each head in the camera to enable motion events. Expected Results … Continue reading Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq

Pelco Motion Notification Could Fail on exacqVision System with Windows Server 2012

A Pelco Pro Sarix camera (IMP-1110) failed to send motion notifications on a Windows Server 2012 system running the the Explicit Congestion Notification (ECN) service. The ECN service and Pelco plugin use the same TCP port 8575; if the ECN starts automatically after system startup, the notification subscription from the Pelco plugin can fail, meaning… Continue reading Pelco Motion Notification Could Fail on exacqVision System with Windows Server 2012