The Pelco NET 6516 encoder experiences interruptions in the footage when used with Exacq Server version 24.12

Description  When installing the Pelco NET 6516 encoder and using Exacq server version 24.12, you may experience interruptions in the footage. Steps to Reproduce  Install Pelco encoder NET 6516 with Exacq server 24.12.0 to 24.12.7 Expected Results  You should see footage without any interruptions from the playback. Actual Results  You will see interruptions in the… Continue reading The Pelco NET 6516 encoder experiences interruptions in the footage when used with Exacq Server version 24.12

IP Plugin Overrides

The standard form for exacqVision camera addresses is as follows: {host}{?parameter_1=value_1}…{?parameter_n=value_n}{#override_1=value_1}…{#override_n=value_n} <br><br> Overrides PluginOptionUsageACTitransport=httpHTTP stream support for legacy platforms and user dataACTitransport=rtspRTSP stream with separate metadata socket for motion/input trigger/video loss/etc.Axiszoom=configBy default zoom only cameras support.Axiszoom=operationForce zoom only operation and controls as part of PTZ and live view.Axisblocksize=offOn by default, but could turn off blocksize… Continue reading IP Plugin Overrides

Pelco Sarix Firmware Version 3.29 Disables Motion Masks in exacqVision 6.2

Introduction Pelco’s release of firmware version 3.29 for the Sarix Professional Series has disabled the creation of motion masks in exacqVision 6.2. Exacq recommends that you do not upgrade to Pelco firmware version 3.29. <br> Process to fix issue If you have already upgraded the firmware, use the camera’s web configuration page to define motion… Continue reading Pelco Sarix Firmware Version 3.29 Disables Motion Masks in exacqVision 6.2

RS-422 Advanced PTZ Menu Control

In version 4.1 of the ExacqVision software, advanced RS-422 PTZ controls were implemented for Pelco-D and American Dynamics domes. One of the advanced controls allows the operator to open the dome’s internal menu to display menu choices in an onscreen display (OSD) embedded in the dome’s video stream. A cursor can be moved up and… Continue reading RS-422 Advanced PTZ Menu Control

Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control

ExacqVision Hybrid servers have the ability to integrate with Pelco Coaxitron CXTA 9760 devices. This allows customers with existing Pelco PTZ cameras that are controlled through the coax with the Coaxitron protocol to be controlled using ExacqVision software. The CXTA accepts the Pelco 422 protocol from the ExacqVision server, and it outputs the data over… Continue reading Connecting an ExacqVision Hybrid System to a Pelco Coaxitron Translator for Analog PTZ Control